Cancel
Showing results for 
Search instead for 
Did you mean: 

Can we create user-defined path in exploded view for rotation.

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

We have the camera path option but form that we can not create user defined path. In camera path option it only highlights existing path which gets created by using flyaround option or built in named views.

3 REPLIES 3

Re: Can we create user-defined path in exploded view for rotation.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Krunal,

 

You should be able to do this using the 'Motion Path' command on the Animation Editor. This command will allow you to select multiple parts and then create a custom path by drawing the curve of the path or selecting keypoints for it to pass through. It will only move the selected parts along that path, so if you want everything to move that way, you will need to select all of the parts. You can create multiple user-defined paths this way. You can find the command here:

 

motionpath.png

 

Hope this helps,

Greg

 

 

Re: Can we create user-defined path in exploded view for rotation.

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

But can we create/import path form sketch tool.

Re: Can we create user-defined path in exploded view for rotation.

Siemens Phenom Siemens Phenom
Siemens Phenom

Unfortunately, I don't think you can.