Cancel
Showing results for 
Search instead for 
Did you mean: 

Can we zip part and assembly files so they can be emailed?

Valued Contributor
Valued Contributor

What is the best way to reduce files sizes so that they can be emailed? I thought could reduce part file size, by rolling back all the way to the top but that only reduces the file size by about 5%. Is there any other tricks to getting the file sizes down?

Regards

Peter

6 REPLIES

Re: Can we zip part and assembly files so they can be emailed?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Compressing is the only thing I know. Or ask the recipient if they have an FTP site you could use.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Can we zip part and assembly files so they can be emailed?

Community Manager Community Manager
Community Manager

I would only ask why email in 2016? Dropbox is much easier for this kind of thing. Even the free account should give you plenty of space to connect with your end client.

Dan Staples
Director, Solid Edge Product Development
Highlighted

Re: Can we zip part and assembly files so they can be emailed?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That's true. Even though I use cloud storage for personal stuff I hadn't considered it for work related stuff.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Can we zip part and assembly files so they can be emailed?

Valued Contributor
Valued Contributor
My only excuse for still using email is that I am a dinosaur. Dropbox does make more sense!

Re: Can we zip part and assembly files so they can be emailed?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yea, and it get's around trying to e-mail files that some e-mail servers strip out like DLL's or EXE's.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: Can we zip part and assembly files so they can be emailed?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Yes, rolling back features is an old trick that can still be used to reduce part file size.

Take any part from the Training folder and the part file can be reduced easily by 30 to 40%

I created the Feature Toggler macro solely for this purpose.

Further you can use the Pack-n-Go program to zip up a set of part files or all files of an assembly at once.

Both programs can be downloaded from here.

 

~Tushar