Cancel
Showing results for 
Search instead for 
Did you mean: 

Can you customize the mouse scroll setting to reverse zoom? Push vs. Pull function.

Experimenter
Experimenter

I have been unable to locate a setting or menu to change. Is it an option?

Thanks

3 REPLIES

Depends on the mouse. On mine i had to change it from doc...

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Depends on the mouse. On mine i had to change it from doc flip to other. Then it work in SE

Re: Depends on the mouse. On mine i had to change it from doc...

Experimenter
Experimenter
is there anything within Solid Edge? I know Solidworks & AutoCAD have the option within the program. Tried various settings with the mouse but nothing worked.

I do not believe there is a setting to change this.  It i...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I do not believe there is a setting to change this.  It is set up similar to 3D motion devices in that you change the perspective of the object, not the perspective of the camera.  This means that you are stationary and you PULL the object closer or PUSH it away.



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com