Cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot download

Experimenter
Experimenter

Hello

 

Can you please help me. I received an email with student licence for SolidEdge program. I tried to download it last week but when I click the English version of the program to start download it doesn't start. The file looks like it is downloading, but the process doesn't move from 0%.

 

Tried also today and with different browsers. Do you have any suggestions?

 

Thank you and BR

Marko

2 REPLIES

Re: Cannot download

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there Marko,

 

The installation file is quite large at 2GB, so if your internet connection speed is not very high, this will take a long time to react....else, if your speed is good, then perhap there has been some background issues on the Siemens download server.....can only suggest you keep trying, and no doubt one of the admin's will spot this post, and be able to offer something more.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Cannot download

Experimenter
Experimenter

Hy

thank you for your suggestion. I managed to download the file from a different location (IP). Maybe it was a problem with my network, but the download did not want to start.

Thank you and BR.