Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Cannot get Solid Edge st9 to run on laptop

"SX" worked finally!  I was able to extrude something!

 

It doesnt transition as smoothly as say my 16GB workstation, but at least its working now!  Ill look at view transitions and stuff to maybe make it perfrom faster on this laptop.  any suggestions you guys?

Owner: Scott Lester Drafting & Design
Designer: Rotork Instuments

Re: Cannot get Solid Edge st9 to run on laptop

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There are some things you lose when not using the Hardware driven options, and performance will suffer.  Don't have any recommendations as we are running workstation cards and thus are always using Hardware driven (advanced).  All has to do with the Graphics adapter your PC has in it and the correct and up to date driver being installed.

 

And is this the graphics driver you have installed?

https://downloadcenter.intel.com/download/25977/Intel-Graphics-Driver-for-Windows-15-33-?product=814...



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Cannot get Solid Edge st9 to run on laptop

Siemens Phenom Siemens Phenom
Siemens Phenom

FYI, the Intel HD 4000 is an integrated GPU so uses the system RAM for graphics processing.  You can tweak the graphics settings to allocate more of your 8 GB system RAM to the video card -- this may help with your overall graphics performance.  Of course allocating more RAM to graphics then reduces the amount of RAM available to the OS and Solid Edge.  Such is the way of integrated GPUs :-( but you may be able to find a happy medium between OS and graphics RAM.  That or upgrade to 16 GB RAM...

Re: Cannot get Solid Edge st9 to run on laptop

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@uk_dave Would the memory allocation (or lack of) stop it from displaying a blank PAR file though?



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Cannot get Solid Edge st9 to run on laptop

I ran the Intel Driver Update Utility and used the one it recommended

 

Owner: Scott Lester Drafting & Design
Designer: Rotork Instuments

Re: Cannot get Solid Edge st9 to run on laptop

Siemens Phenom Siemens Phenom
Siemens Phenom

@KennyG no I would not expect increasing the video RAM to resolve the not being able to open a new .par file but my comment was in response to @scott_lester's comment...

 

It doesnt transition as smoothly as say my 16GB workstation, but at least its working now!  Ill look at view transitions and stuff to maybe make it perfrom faster on this laptop.  any suggestions you guys?

Re: Cannot get Solid Edge st9 to run on laptop

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@uk_dave  I was assuming that was because he was running in "Software driven".



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Cannot get Solid Edge st9 to run on laptop

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@scott_lester I don't know much about the Intel embedded HD graphics, but I do believe the model you have supports OpenGL and should work in "Hardware driven", but it has to be the correct driver for Windows 10.  The one I posted was the latest I could find for the HD 4000 graphics for Windows 10.  If it is newer than the version you have installed, then I would try it.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com