Cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot start the program

Not applicable

Each time that I attempt to start SE2D the "startup wizard" comes up, & the program
never boots up. (PC using Vista)
Mike
1 REPLY

Re: Cannot start the program

Not applicable
Mike,
What version of Vista are you running? (Home Basic, Home Premium,
Professional)
Did it install properly? The executable you downloaded is for installation
only.
Did you allow the additional Microsoft components to install when prompted
during installation?
When you say you see the startup wizard and it never boots up, are you
clicking on Solid Edge 2D Drafting under the Start menu? The reason I ask is
because there is no startup wizard. The program will start without any user
interaction.
Regards,
Rick B.