Cancel
Showing results for 
Search instead for 
Did you mean: 

Cartesian coordinate dimensioning ORIGIN BS 8888 / ISO128

Pioneer
Pioneer

Dear community,

 

I'm trying to place the origin in the coordinate dimension of a hole table. As you can see have no problem stabilising the circle in the 103mm dimension to stablish the origin of it (see image).  The problem is trying to do the same to the X1 axis. Can anyone put some light on how to activate the circle in the XY1 coordinate system?

 

HOLE TABLE ORIGIN.png

 

 

Best,

Josue

6 REPLIES

Betreff: Cartesian coordinate dimensioning ORIGIN BS 8888 / ISO128

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @JosueVivas

 

 

 

is it possible to formulate Your request a little bit more in detail.

 

What exactly should be done how and where?

 

 

regards
Wolfgang

Betreff: Cartesian coordinate dimensioning ORIGIN BS 8888 / ISO128

Pioneer
Pioneer

Hello @hawcad,

 

According to the BS 8888 "the origin of the coordinate dimension shall be indicated". There should be a circle establishing the origin of each axis for the hole table as seen in the picture below. I can't put a circle in the coordinate dimension in SE. or modify the location of the X1 and Y1 labels. I hope that now makes sense. Thanks.

 

 

 

IMG_3750.JPG

Highlighted

Betreff: Cartesian coordinate dimensioning ORIGIN BS 8888 / ISO128

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @JosueVivas

 

 

 

OK, understand and in a hurry I have not found any basic setting to achieve that for the origin marks of a hole table.

 

What You can do is to add a single coorinate dimension (base only) to show that this is the origin of Your coordnate dimensions and the hole table.

 

20180525_1221.png

 

As You can see, to place both exactly I have turned on a grid!

 

 

regards
Wolfgang

Betreff: Cartesian coordinate dimensioning ORIGIN BS 8888 / ISO128

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi @JosueVivas,

The way shown by our great community asset @hawcad, is as I found also.....but further to this, you can also choose not to display the coordinate dimension text, leaving only the circle.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Betreff: Cartesian coordinate dimensioning ORIGIN BS 8888 / ISO128

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @SeanCresswell

 

 

of course and absolutely Yes.

But I thought that this is nothing to be mentioned extra.

 

So if You like this to have just change the dimension to .

 

20180525_1536.png

 

 

Thanks to You @SeanCresswell for pointing to this issue!

 

 

regards
Wolfgang

Betreff: Cartesian coordinate dimensioning ORIGIN BS 8888 / ISO128

Pioneer
Pioneer

Hello @hawcadand @SeanCresswell,

 

Thanks for the input, this helped.

 

It's a shame that the user has to find a walkaround to comply to ISO 128. Does this mean that SE is not ISO ready? With so many years in the market, I find it hard to believe. Anyways, we have the short route thanks to you guys. 

 

Best,

Josue