Cancel
Showing results for 
Search instead for 
Did you mean: 

Center Axis Size and Color

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

For years I've been dealing this long issue long enough. I can't see the center of a circle

Basically, the axis of center circumference color has been set with a default as well as the size.

Is not a visual-friendly idea.

 

Thanks

Greg 

1 REPLY 1

Betreff: Center Axis Size and Color

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @PO_LC

 

 

but to be honest, for most SE users for the last 20 years it seems to be still enough center symbol for any circle and arc.

 

BTW, YOu never ever need to sse it anyway, simply press the "C" button when hoovering over an arc with the mous to select the center point.

Doing so, it even isn't necessary to see that center point on screen, but You can select it and use it.

 

 

regards
Wolfgang