Cancel
Showing results for 
Search instead for 
Did you mean: 

Centre mark between holes?

Valued Contributor
Valued Contributor

excuse the ugle centrelines ive drawn with my mouse, but whats the quickest way to add connecting centre marks between holes.

note they're at an angle too.

 

Capture.PNG

Regards,

MagRiz
(ST9 User Est 01.18)
3 REPLIES 3
Highlighted

Re: Centre mark between holes?

Valued Contributor
Valued Contributor

MagRiz,

 

If you select the "Dimension Axis" option when placing a centreline, you can choose a line on the slot say, and then select a hole.

This will give you a centreline at the correct angle.

Or you could choose centreline between two points, and pick the centre point of each hole. Then extend the ends to give the desired result.

Hope this helps. 

Matt Hunt IEng.MIED
Design Engineer
M-Flow Technologies

ST10 MP*
K2200

Re: Centre mark between holes?

Valued Contributor
Valued Contributor

@MattHunt

Thanks, 

 

i've used that method to get the centre marks but there are no points on the ends allowing me to drag out the lines.

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Centre mark between holes?

Valued Contributor
Valued Contributor

@MagRiz

 

Yes you're right, not with centre marks. But if you try 'centrelines' between two points, you should be able to extend the ends.

Matt Hunt IEng.MIED
Design Engineer
M-Flow Technologies

ST10 MP*
K2200