Cancel
Showing results for 
Search instead for 
Did you mean: 

Centrelines - how to hide them

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

another simple question I guess,

 

how to hide the centrelines ( in one go - all centrelines, not one after another ) on the drawing environment ?

 

Thank you,

 

Arek

Centrelines.png

6 REPLIES 6

Re: Centrelines - how to hide them

Gears Phenom Gears Phenom
Gears Phenom

options:  in the view properties like you show, use the query at the bottom to select all then you can hide.

 

best option...  set global setting in SE option to not show center lines...  this must be set before you place the drawing view and will create teh view without the CLs.

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Centrelines - how to hide them

Gears Phenom Gears Phenom
Gears Phenom

Hi @Johnson_BigMatt,

 

can you please show me how to set it up ?

 

What property the centreline belongs to ?

What about conditions ?

 

I am not familiar whith this - is there any instruction how to use it ?

 

thank you,

 

Arek

 

query 1.pngquery 2.png

Betreff: Centrelines - how to hide them

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @arekkul

 

 

 

is the centerline issue a general question or only regarding tubes and frames as shown in the pictures?

 

regards
Wolfgang

Betreff: Centrelines - how to hide them

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @arekkul

 

 

 

sorry, forget the last question.

Centerlines only will be theer when having tubes or frames!

 

Time to take a coffee!

 

Smiley Wink

regards
Wolfgang

Re: Centrelines - how to hide them

Gears Phenom Gears Phenom
Gears Phenom

7-26-2017 9-00-10 AM.png7-26-2017 9-01-04 AM.png7-26-2017 9-03-45 AM.png

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Betreff: Centrelines - how to hide them

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @arekkul

 

 

 

here You can see how tho change the "CenterLine visibility glogal for Your drawing or as shown for one view:

 

20170726_1509.PNG

 

  1. Go to View Properties via RMB
  2. Enter the Drawing View Display Default button and the appropriate form
  3. There You will find (at the bottom) the option for showing tube centerlines or not
  4. Change to no and 
  5. Accept with OK
  6. Afterwards press the "Restore Deafult Display Settings" button in the upper right corner
  7. should be done correctly now

 

In General Draft Options under Annotion, You also will find the global setting for the hole draft

20170726_1514.PNG

 

 

regards
Wolfgang