Cancel
Showing results for 
Search instead for 
Did you mean: 

Century Gothic TTF in PDF

Valued Contributor
Valued Contributor

Has anyone noticed that Solid Edge will not let you save a pdf that uses the Century Gothic font?  Maybe it's an agreement with Solidworks...

6 REPLIES 6

Re: Century Gothic TTF in PDF

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MattS,

 

Just tested that, and seems to work, as expected.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Century Gothic TTF in PDF

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

I am able to save to PDF using the Century Gothic font.

Do you get any error message or it just doesn't create the PDF ?

Re: Century Gothic TTF in PDF

Valued Contributor
Valued Contributor

If I view or print a draft, I get this...

3.JPG

If I create a pdf, I get this...

4.JPG

Using ST8, latest service pack...

 

Matt

Re: Century Gothic TTF in PDF

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

OK, I agree.

My fonts tab shows either Tahoma or some AvantaGarde (which matches when I checked online) and I have no clue how the later comes into picture since it is not installed on my system.

  

I think font mapping, as in the case of DWG, is not exposed yet, hence this appears to be some internal mapping.

 

Highlighted

Re: Century Gothic TTF in PDF

Valued Contributor
Valued Contributor

I can only speculate that Siemens doesn't want their drawings to look like Solidworks.  Kinda bums me out as I think Century Gothic is very clear and easy to read on a drawing.

 

Re: Century Gothic TTF in PDF

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Ah, I see now, it's in the "Callout Text" area.....yes, I get the same result.

 

I remember on my old computer, I had Adobe Pro suite, and the print to PDF functionality it had, also allowed the option to embed fonts. I suspect this is what is happening here, or rather, "not", during the Save As - PDF in Solid Edge.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000