Cancel
Showing results for 
Search instead for 
Did you mean: 

Chain selection..stop at intersection

Phenom
Phenom

I was working in SE Ordered today and attempted to do a similar sketch that I did in ST mode.

 

I have drawn a sketch that consists of full circle and fillets (arcs) inbetween the full circles. I am attempting to extrude the profile but I am finding that the system does determine that I have multiple full loops but is not allowing me to select region points or something similar to determine a region.

Is there either a way to define region(s) or is there a way that the selection function single or chain will recognize an intersection point and allow the user to determine if it is ok to process to the next point in the "chain'?

16 REPLIES

Re: Chain selection..stop at intersection

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

I don't know any solutions for this. Ordered mode dosen't support regions "only" opened and closed profile what are exact (without overlapping, etc...). Synch is more flexible in this case.

 

What I suggest is that you must use sketch command and it has to contains "all selection possibilities". Yes, you must pre-plan this...

 

A video about this:

 

BR,

Imics
http://solidedgest.wordpress.com/
Highlighted

Re: Chain selection..stop at intersection

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

if you dont need the diameters in the corners simply trim off the extents, or if needed,  use the split command to split the diamenter into its 2 segments.

 

hth

Matt Johnson
Application Engineer
Ally PLM Solutions
matt.johnson@allyplm.com
http://allyplm.com/

Re: Chain selection..stop at intersection

Phenom
Phenom

Thank you. Yes, I was able to generate what I needed quickly in ST. I do like the abilities found within ST for regions.

Re: Chain selection..stop at intersection

Phenom
Phenom

Splitting and trim really aren't options that would be very successful for model manipulation in ordered mode- you would lose the tangent points.

 

A still feel that a simple "intersection" definition would be a great enhancement for those of use that still need/want to work in Ordered mode.

Re: Chain selection..stop at intersection

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Ryan,

 

Of course, although it adds another step, you could use a primary sketch, then when extruding, use the "include" command.....it remains trimmed & constrained to the sketch.

[it has been known to be a bit fragile, if downstream geometry changes go beyond the bounds of the trimmed extents & relationships]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Chain selection..stop at intersection

Phenom
Phenom

At each circle join the ends of the tangent curves with a line to create a closed shape - you can then select that and the 4 circles to extrude in one hit.

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.

Re: Chain selection..stop at intersection

Pioneer
Pioneer

When did SE stop supporting regions in ordered? I used SolidEdge prior to Synchronous and found it the best of the mid-range CAD systems. I've recently come back to it and found with ST8 things aren't as they were in V19. Regions were the first big shock, and my mates do not seem to be as robust when changing parts as well. It's almost like Solid Edge is trying to kill ordered.

Re: Chain selection..stop at intersection

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't recall SE ordered ever working with regions. And I've used it off and on since 2001.

Though stop at intersection might be a good idea, a problem is which way does it then go? The high road or the low road?

I suppose it could ask for directions.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Chain selection..stop at intersection

Pioneer
Pioneer

I'm positive V17 through V20 (what I used in college circa 2005-2008) allowed region selections. This was before ST technology. Designing in ST mode feels much more like those versions, but as a design team I do not wish to be the only one using ST. Also, I do not have a good feel for ST in sheet metal design.

 

Regardless, every other mid-major CAD system uses region seletion with history modeling, so I do not in any way understand why it is not there, other than Siemens continously trying to push NX.