Chamfer Conundrum

Pioneer
Pioneer

I am working on a foot for a trestle table, I want to add a chamfer along the two top edges, but I also want the chamfer to end about mid-way along the top of the foot where the leg will attach.

 

Being fairly new to SE I not sure how to create the end the chamfer so that it represents the way it will look when the chamfer is created using a router, the end of the chamfer should be a small tapering radius ending in a point.

 

I have attached .pdf of the foot to show where I am stuck, you can see the the chamfer terminates in a squared-off fashion.

 

Thanks in advance for any help.

4 REPLIES

Re: Chamfer Conundrum

Esteemed Contributor
Esteemed Contributor

Hi there,

 

I think the easiest way would be to allow the chamfer to run the entire edge, then make a protrusion to replace local the area for the leg landing...use a vaiable radius fillet to get your router blend.

 

SECommunity_ChamferConundrum.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Chamfer Conundrum

Phenom
Phenom

The method Sean used is no doubt the easiest.

Another approach would be to use a derived curved and a triangular cross-section sketch used to create a swept cutout. This may not need adding material after the cutout but extra steps will be required to create the derived curve. The fillet at end is of regular type.

 

Untitled.png

Re: Chamfer Conundrum

Pioneer
Pioneer
Thanks Sean I will this a try.

Re: Chamfer Conundrum

Pioneer
Pioneer
Thanks Tushar. I am going play around with your suggestion.