Cancel
Showing results for 
Search instead for 
Did you mean: 

Chamfer Solution

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello Averyone,

 

please advice on how to successfull make a 3mm chamfer on highlighted edges chain.

 

it's coreblock created with moldtooling

 

Untitled.png

1 REPLY

Re: Chamfer Solution

MLombard
Retired

You could extrude a surface up to the the face of the block, and then make a ruled surface from the edge, using the ruled surface to cut the corner off the block.

 

Or just project a sketch onto the block and do the same thing.

 

You could sweep an angled line (as a surface) around the block using the square base as a path but using the top edges as the guide curve. This should give you a surface to cut the edges off with.

 

Offset the top edge 3mm on each side, and extrude that at an angle of 45 deg, and do it on all 4 sides.

 

Assuming you'd cut the chamfer with a wire edm?

Retired Community Manager for Solid Edge. This account is no longer active.