Cancel
Showing results for 
Search instead for 
Did you mean: 

Chamfer on double(?) curved surface/line

Creator
Creator

Dear Members,

 

I m asking your help in the following matter.

I would like to make a chamfer on the selected edge (see 1st image). This plate is 5 mm thick. The chamfer should be 60 degree and 4 mm setback, so the bottom edge of the cutout should be 1mm thick all around.

But anyhow I try to make the chamfer I am unable to accomplish, see the 2nd figure. You can see that the bottom edge(surface?) is made with a variable width., not a constant 1mm.

This plate is a strengthening to a flange.

What should I do? How should I do?

 

Any help is appreciated because I m stuck with this.

Without chamfer.jpgWith chamfer.jpg

17 REPLIES 17
Highlighted

Re: Chamfer on double(?) curved surface/line

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Maybe a swept cut? Could you attach the part file?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Chamfer on double(?) curved surface/line

Creator
Creator
I have attached the file, I also tried the swept cut, but without succes.

Re: Chamfer on double(?) curved surface/line

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'd bet that @Imics or some other guru will come through. Fridays are slow around here so maybe not until next week.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Chamfer on double(?) curved surface/line

Genius
Genius

Hi @magiclevinho try this solution.

 

(view in My Videos)

 

Regards.

Re: Chamfer on double(?) curved surface/line

Pioneer
Pioneer

Just curious - what do you imagine the end result to be?

 

 

Looking at it, I do not think you'll find a real solution where it acts exactly like a 60° chamfer you'd find on a flat part. Because you've cut normal to the surface of your curved part, your 5mm thickness is variable along the path. You'll need to define your 1mm height and let the cut height "float" above the top surface of the part.

 

There might also be an issue maintaining a 60 degree chamfer - it has been a while since I have played with curvelinear surface geometry - so I can't remember if you can maintain a 60 degree cut at every normal plane to your path or if that angle has to float as the path "rises and lowers" to where your cut plane is.

 

You're in some nasty geometry territory - have fun!

Re: Chamfer on double(?) curved surface/line

Pioneer
Pioneer

Yep - you can't use a vertical line normal to the cut... it would leave remanents inside the sweep. That makes absolute sense.

Re: Chamfer on double(?) curved surface/line

Creator
Creator
Thank You very much! I will make like this!

Re: Chamfer on double(?) curved surface/line

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Kanwulf, Nice! Seems like the offset and intersection are not necessary though. It can be done with a plain old sketch on a base reference plane.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Chamfer on double(?) curved surface/line

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

I know, I was late for the party. Smiley Very Happy @Kanwulf's solution is perfect. I don't know who knows that Blend provides chamfer option for similar cases... Just a suggestion, no more!

 

Here is a video:

 

BR,

Imics
http://solidedgest.wordpress.com/