Cancel
Showing results for 
Search instead for 
Did you mean: 

Change Inertia Values from kg m^2 to g mm^2

Creator
Creator

Hi

 

How can one change the Inertia variable units from kg m^2 to g mm^2? 

 

There is no option in the file options command to change inertia value found physical properties.

 

See image attached for specific units (highlighted) in question.

 

Thanks

2 REPLIES 2

Re: Change Inertia Values from kg m^2 to g mm^2

Siemens Phenom Siemens Phenom
Siemens Phenom

MisterHon,

you change this in 'settings/options/Solid Edge Options/Units'.

 

Change to Mass Unit = g and you will get the Inertia in g-mm2.

 

Good luck!

 

/ulf

Siemens EMEA GTAC Support

Re: Change Inertia Values from kg m^2 to g mm^2

Creator
Creator
Prompt response is appreciated