Cancel
Showing results for 
Search instead for 
Did you mean: 

Change dimension scroll increments

Valued Contributor
Valued Contributor

So when i add a dim and scroll up or down, the increments change, but to weird numbers. i want to change that so when i scroll the increments are 1mm instead. 

 

how?

 

Regards,

MagRiz
(ST9 User Est 01.18)
7 REPLIES

Re: Change dimension scroll increments

Gears Phenom Gears Phenom
Gears Phenom

AFAIK, and Sadly, there is no way to modify the increment of this dynamic change.

 

certainly worth an ER IMO!


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Betreff: Change dimension scroll increments

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

 

the change value is not a real weird one, but always 5% of the start value

So if Your start value is weird, any changes are it too.

 

 

regards
Wolfgang

Betreff: Change dimension scroll increments

Valued Contributor
Valued Contributor

@hawcad but my start value isnt weird. if it start at 72mm why would i want the next increment to be 75.6 (@5%)??

logically it would go up in whole/ round numbers. 

 

i think any manufacturer would prefer 75mm over 75.6mm

Regards,

MagRiz
(ST9 User Est 01.18)

Betreff: Change dimension scroll increments

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

of course You would prefer 75mm, but 5% of 72mm are 3.6mm and so the result is 75.6mm

 

I think it gets hard to find a solution for any situation.

If I start scrolling a base value of 1000mm and it scrolls in 1mm steps I would not be happy.

Same if I start with 0.2mm and recieve 1.2, 2.2 and so on as result, would not make You really happy.

 

 

regards
Wolfgang

Betreff: Change dimension scroll increments

Valued Contributor
Valued Contributor

@hawcad

but my point is it doesnt make sense to do it that way.

and this is where having an option in the little pop up window allowing you to change the increments would be ideal, exactly like SW (you type what increment you want or use the defaults ranging from 1to 10 i think).

even if it was 1mm at 1000mm thats fine as using the scroll function only makes sense for small changes. if i want to add 250mm id just type that in as a formula - not scroll 250 times.

Regards,

MagRiz
(ST9 User Est 01.18)

Betreff: Change dimension scroll increments

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @MagRiz

 

 

I fully understand Your wishes, but only wanted to explain how it has worked till now.

And I personally use the scroll change of a dimension for controlling how a modification/change will influence the geometry, and how stable all my realtions are.

 

So I'm very happy with the 5% step independend of the absolute value.

 

And an absolute step value can be defined for all mous operations for extrusion length, etc.

If there is a value of 10mm or 5mm the increments will be exact and round numbers.

 

 

regards
Wolfgang

Betreff: Change dimension scroll increments

Creator
Creator

This was very simple in SolidWorks--there was simply an option to update the dimension scroll increments. I would set mine to .0625 or .125 for 1/16ths or 1/8ths of an inch. 

 

I'm not sure what's difficult about this for Solid Edge. It sure improved the User Experience and how fast it was to enter dimension changes.