Cancel
Showing results for 
Search instead for 
Did you mean: 

Change flange from outside bend to inside?

Valued Contributor
Valued Contributor

Hi,

 

How can someone change a flange tab from outside bend to inside?

3 REPLIES

Re: Change flange from outside bend to inside?

once you select teh face of the flange you are presented a vector arrow.  this is the steering wheel.  simply select that vector and move the face up...

 

you mention in you r video that you can not find the feature settings to toggle from outside to inside bend.  this is THE difference between Ordereed (history based modeling) and Synchronous (non history based)  in sync once a feeature is created you are only dealing with face sets.

 

if you want to deal with features then you need to be in ordered mode.

 

Re: Change flange from outside bend to inside?

Phenom
Phenom

No sure if this is what you're after, but like many things in Sync, there are other ways to fix issues such as yours that was more straight forward in Ordered.

 

watch this and see if this helps:  http://screencast.com/t/88X0ouN1

 

Bob

 

 

Re: Change flange from outside bend to inside?

Valued Contributor
Valued Contributor

Ahhh, i'm starting to see the difference between Ordered and Sync. now.

Thanks a lot guys, it's working now Smiley Happy