Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Change ribbon menu and pathfinder fonts - SE6 and WIN7

Gears Phenom Gears Phenom
Gears Phenom
I'm not aware of any guideline about mess with the registry cause it is highly recomended to not touch it.

Since you were so desperate about this customization I only suggested to have a look at the registry and see if there is any key font related.

What each keys does is a Hustville guys things, so unless some of them would explain a bit it is a DIY thing.

Re: Change ribbon menu and pathfinder fonts - SE6 and WIN7

Valued Contributor
Valued Contributor

Do not afraid Sir. I dont want to do a mess in reg.
Yes, I will explore reg in this weekend for a bit. I hoped there is any guideline for regedit SE.

Who are Hustville guys? Where I should snif them?

Re: Change ribbon menu and pathfinder fonts - SE6 and WIN7

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

On the Helpers section of the Options, you can increase button size by 2X which also increases the font size.  Aside from that, you can use the Windows Font Scaling which I'm not certain will work everywhere within SE.

font scaling.png



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Change ribbon menu and pathfinder fonts - SE6 and WIN7

Valued Contributor
Valued Contributor

Grundey,

 

Thanks for your suggestion, I have tried it before. DPI is not what I want. Change Only font for pathfinder and upper ribbon bars.

 

If its in the register I cant find it..Anybody? I'm loosing hope.

Re: Change ribbon menu and pathfinder fonts - SE6 and WIN7

Valued Contributor
Valued Contributor

Good news,

 

Finally I have found it. The both fonts - ribbon bar font and pathfinder font now are decreasing or increasing, in the same measure.

 

HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge\Version 106\DEBUG\Ribbon Bar Font Height

 

Thanks anyway. 

 

CB

Re: Change ribbon menu and pathfinder fonts - SE6 and WIN7

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

excuse me, you mean that this method make front size in ribbon bar change???

due to my ribbon bar has small size as cannot see.

Re: Change ribbon menu and pathfinder fonts - SE6 and WIN7

Experimenter
Experimenter
Great fix. Thank you.

Re: Change ribbon menu and pathfinder fonts - SE6 and WIN7

Please,

I´ve got the registry key but I don´t know what should I change.

Tks!

Capturar.JPG