Change section hatching

Honored Contributor
Honored Contributor

When I go into the display properties of a section view, the option to change the hatch pattern is grayed out.

 

What switches do I need to use to allow me to change the hatch pattern for cross sections of steel. I want to use a solid fill rather than the standard hatch pattern because I have many sheets at 45 deg to the world that the 45 deg hatching does not work well.

 

 

7 REPLIES

Re: Change section hatching

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

The section property is controlled by the part material. So to change the hatch pattern you need to edit the part's material properties.

Cheers

Mark

Re: Change section hatching

Honored Contributor
Honored Contributor

I was hoping to edit the hatch for just this single drawing, not every time I use my most common material.

Re: Change section hatching

Esteemed Contributor
Esteemed Contributor

Hi Scott,

 

Alternatively....if this is a one off, rather than editing the models material definition.....what I do is use "Draw in View" and edit the displayed hatch properties there. [color, direction, spacing, etc....]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Change section hatching

Honored Contributor
Honored Contributor

Good work around. I should be able to just turn off the section hatching and then use old drafting methods.

Re: Change section hatching

Phenom
Phenom

The drawing view Properties > Display tab gives you some control over hatching.

You can turn all on/off, change style, set spacing and angle for all parts, multiple parts, or you can dig down to a single part and apply to that one only

HP Z420 16GB RAM
Quadro K4000
ST10 MP3 on Windows 10 Pro 64.

Re: Change section hatching

Honored Contributor
Honored Contributor

That's what I'm trying to do. I could not figure out what switches needed to be touched in order to edit the hatching style......for anything. Unless I go edit the material.

 

When you open that window, by default the hatching style is set to the material and grayed out.

 

I'm hoping for a draft file specific solution. Perhaps there is not one.

Re: Change section hatching

When you go into the properties of that view, you can go to the Display tab, and there should be a checkbox to uncheck that tells it to use material.  Once you uncheck it, right above it, the grayed out hatch style box will become available to choose as you want.

Owner: Scott Lester Drafting & Design
Designer: Rotork Instuments