Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Re: Changing Background with Macro

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG

 

 

first let me say, that I 100% agree with Your coment that those settings should/must be user specific.

Anything else leads into problems with old files, different user requests regarding the UI and so on.

 

A centralized setup for all those options and settings might one of the biggest enhancements we can wish for Solid Edge.

 

OK, there was a beginning seen with the ST9 Setting and Prefrence wizzard, but at the same time I was happy with this new function I had stop to use it, due to the fact that the current user name is completely stored and used for registry settings.

So man can not use this feature for a rollout of company settings for SE.

I still continued to use my own old scripts which handle that IMHO better and easier than the rollout function of ST9

 

Here is a big point for enhancement.

 

 

 

And now let me say thanks for offering sharing the view style code what I gratefully would like to recieve

 

Thanks

 

 

regards
Wolfgang