Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Changing Radius to Diameter

Creator
Creator

Currently if I select a circle the radius value is highlighted by default in the "Edit Definition" window. Is there any way to change it so when I select a circle the diameter value is highlighted instead?

 

2 REPLIES 2

Re: Changing Radius to Diameter

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I do not believe so.  If you hold Shift and hit the Tab key, it will become the focus, but there is no way to make the focus the default for the command.  That would require logging an incedent report with Siemens if you are on maintenance.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Changing Radius to Diameter

Creator
Creator

OK, thanks for the response. I kind of figured that was the case.