Cancel
Showing results for 
Search instead for 
Did you mean: 

Changing from part to part In-place edit

Phenom
Phenom

When I move from editting (in place) one component to another in the same sub-assy I notice that the display needs to move up to the sub-assy and then drop back down into the component. Why is this?

4 REPLIES

RyanM,   Don't need to go back to sub-assy! ;)   If you e...

Gears Phenom Gears Phenom
Gears Phenom

RyanM,

 

Don't need to go back to sub-assy! Smiley Wink

 

If you edit a part from assembly then you can change "edited part" with double click (or RMB and Edit) on the "part name" in Pathfinder...

 

Here is a little help:

 

 

BR,

Imi

Imics
http://solidedgest.wordpress.com/

Re: RyanM,   Don't need to go back to sub-assy! ;)   If you e...

Phenom
Phenom
LMI-

Thanks for the video. I do understand how to make changes for part to part. What I was wondering was why I see the flickering and notice that the assembly has to activate to move to another component in the same assembly. Your video actually shows this flickering happening for you. I have a slow i7 laptop so I definitely see this lag/flickering.

Re: RyanM,   Don't need to go back to sub-assy! ;)   If you e...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What's happening there is, [approximately] it's saving/closing/returning/opening/updating, etc.....between files & their respective states. Obviously the less powerful the hardware, the more of this activity is made visible.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: RyanM,   Don't need to go back to sub-assy! ;)   If you e...

Gears Phenom Gears Phenom
Gears Phenom
RyanM,

Sorry, but I don't know the reasons, but maybe Dan knows the answer. Smiley Happy

Yes, it is a bit flickering.

BR,
Imi
Imics
http://solidedgest.wordpress.com/