Cancel
Showing results for 
Search instead for 
Did you mean: 

Changing properties of a section arrow.

Phenom
Phenom

Is there a way to change the default settings for a section (and view) arrow?

I would like to change the aspect ratio of the arrow head to make it a little wider, and shorten the length of the arrow line to be about 2x the arrow length.

I know you can drag the end of the line to change it when placed.

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.
2 REPLIES

If you want this to apply to Cutting Plane Lines only, th...

Community Manager Community Manager
Community Manager

If you want this to apply to Cutting Plane Lines only, then you need to use "Style Mapping" which allows you to do styles that differ by elements type. First, set up a Style (ISO Section Lines or something) that has the properties you want. Then go to Options > Drawing View Styles  and turn on Style mapping and make sure the cutting plane line points to your new style.

Dan Staples
Director, Solid Edge Product Development

Re: If you want this to apply to Cutting Plane Lines only, th...

Phenom
Phenom

Thanks Dan, but it isn't the line I want to modify.
All arrow heads are basically the same shape - width is about 1/4 x length. and although section arrows are bigger they can be difficult to distinguish from dimension arrows on a complex drawing.
I want the arrow to be wider - about 2/3 x length as shown below - but there is no way to generate a different arrow head style

Capture.JPG

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.