Cancel
Showing results for 
Search instead for 
Did you mean: 

Changing size in 2D Drafting 2019

Experimenter
Experimenter

stars size.jpgI would like to change the size of a 2D object in Solid Edge 2D Drafting 2019 free version.  In the attachment: how can I set size of the star from 113,38 mm to 50mm? SE only allows to make smaller one line. How can I make the whole star smaller? I have used Autocad in the past and now also would like to save files as dxf.

5 REPLIES 5

Re: Changing size in 2D Drafting 2019

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

With a shape like that it might be easier to scale the whole thing. Otherwise you would need to create many relationships and dimensions to parametrically control the shape. With simpler shapes like squares, hexes, etc. it's not hard.

If you just set up half of it with parameters then mirror it it would be easier.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200
Highlighted

Betreff: Changing size in 2D Drafting 2019

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @pompi 

 

 

 

this is a video, showing what @bshand  mentioned already.

 

Select th ecomplete star and scale this geometry to the wanted value.

The scale factor is "Result divided by current value"

 

(view in My Videos)

 

 

Sorry for the German SE and for the irregular star!

 

regards
Wolfgang

Betreff: Changing size in 2D Drafting 2019

Experimenter
Experimenter

Thank you, Bruce!

 

Thanks a lot, Wolfgang!! The video is perfect for me who is a total amateur!! Smiley Happy The star is marvelous Smiley Happy

Betreff: Changing size in 2D Drafting 2019

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@pompi 

Kindly mark all relevant replies you think as 'Accepted Solutions'.

This will give due credit to contributors and help other users in the future.

I believe you will also receive an automated email with a similar message in a short while from the forum.

Betreff: Changing size in 2D Drafting 2019

Experimenter
Experimenter

Sorry - it is done! Smiley Happy