Cancel
Showing results for 
Search instead for 
Did you mean: 

Changing the colour of multiple callouts

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

Can you tell me please how to change the colour of a few seperated callouts in one go ?

 

thank you,

 

Arek

5 REPLIES 5

Re: Changing the colour of multiple callouts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @arekkul,

 

You can multi select them [with +CTRL] then go to properties to change colour there, and it will update all selected call outs.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Changing the colour of multiple callouts

Gears Phenom Gears Phenom
Gears Phenom

Hi @SeanCresswell

 

hope you are well.

 

Yeap, I knew this method but coudn't change it this way.

After a few attempts I have done it properly.

 

But you cannot use the RMB to apply Properties - it is only changable using command on the ribbon.

 

Thank you 

regards,

Arek

Re: Changing the colour of multiple callouts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yes I am well, thank you @arekkul.

 

Ah yes, good point, I forgot to mention, RMB drops the select set to the local selection.....must use the ribbon to access.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Changing the colour of multiple callouts

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi @arekkul

  

Further to what @SeanCresswell suggested, after using the Ctrl key for selecting multiple callouts, continue keeping the Ctrl key pressed and 'Double-Right-Click' on the selection to get the context menu from where you can select 'Properties'.

  

Bit clumsy, but it works.

  

Tushar

Re: Changing the colour of multiple callouts

Gears Phenom Gears Phenom
Gears Phenom
Thank you @Tushar.

regards,

Arek