Cancel
Showing results for 
Search instead for 
Did you mean: 

Changing the orientation of downloaded model?

Hey guys.

 

I hope you can help me.

 

I want to know if there is a way to change the orientation of a part or model you downloaded.

Sometimes the orientation will be completely wrong and it messes everything up.

 

Hope you guys has some tips I can use.

 

Thank you

6 REPLIES

Re: Changing the orientation of downloaded model?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In Synchronous select the part or assembly (assy would be the same in ordered) and rotate it using the steering wheel after selecting the correct axis. It may require two rotations to get it the way you want it. You also might want to move it to get it situated on the coordinate axes.

In ordered you should be able to use Home/modify/rotate faces then select body.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Changing the orientation of downloaded model?

Legend
Legend

Christaan.

 

The way I do it and this may not be the best or quickest way, is via insert part copy

Open the downloaded file in SE and save as PAR.

Open a new PAR (in ordered) and use the abilities with either a mirror or a different coordinate system.

Once the 3D model is in the correct orientation, move all to synchronous (breaking the link to the original) and voila, you have the e3D model in the orientation you want it to be....

--------------------------------------------------
Marc Boom
marc.boom@outlook.com

Re: Changing the orientation of downloaded model?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Always more than one way to skin the proverbial cat.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Changing the orientation of downloaded model?

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Another way to skin the cat is to pull the downloaded part into a new blank assembly and assemble it into the desired orientation.  Then save the assembly out as a parasolid and pull it back into SE again as a part and save.  You will then have the part in the desired orientation.  Clean and simple with a minimal feature tree just like the original downloaded part.

 

As an aside -- if the downloaded part is actually an assembly and you are going to convert it to a single part -- and you wish to alter the colors of the parts, do it before saving out to the parasolid mentioned above.  It is often easier to change the colors at this stage rather than tediously selecting faces in the single part later on.

Re: Changing the orientation of downloaded model?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@chrisstandring, It's only "clean and simple" if you want to maintain it in ordered. Cleanest and simplest is synchronous IMO.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Changing the orientation of downloaded model?

Thanks for the input guys.

 

I ended up using only the "rotate face: function and it worked like a charm.