Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Changing visible icons

Pioneer
Pioneer

Hi,

 

On ST10, is there any way of changing which icon is the default visible one on the toolbar?  For example, on Sketch (in Ordered), I use frequently use Rectangle by 2 Points, and rarely use Rectangle by Centre. Is there a way of switching it around so the one I use is visible on the toolbar, without having to go through the drop-down menu each time?

 

Many thanks in advance!

7 REPLIES 7

Re: Changing visible icons

Gears Phenom Gears Phenom
Gears Phenom

you have 2 options,

 

1.) customize the toolbar to show the tools you prefer

2.) set the option for last used on top.  this will keep the "by 2 points" on top of the pull-down for 1 click access.  This is not recalled between sessions however IIRC.  so you will need to select it 1x each session

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Changing visible icons

Pioneer
Pioneer

Thanks for the reply.

 

I've gone into the Customise Toolbar, and expanded to see the tool and drop down. I even managed to shift up the Rectangle by 2 Points so it is at the top, and saved it as a New Theme 1 (see attached).

 

However, I can't get it to become visible without expanding the drop down menu.  What do I need to do?

Re: Changing visible icons

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

I'd suggest customizing the ribbon to create the 'Rectangle by 2 Points' icon as a separate tool and ignore the pull-down.

Re: Changing visible icons

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

To elaborate on @Tushar's comment:

 

rect2points.png

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Changing visible icons

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Right. That's what I meant.

Thanks Bruce.

Re: Changing visible icons

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Tushar, Well I already did the work when I noticed your post. So I posted it anyway.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Changing visible icons

Pioneer
Pioneer

Thank you everyone for your help!