Cancel
Showing results for 
Search instead for 
Did you mean: 

Changing visible icons

Pioneer
Pioneer

Hi,

 

On ST10, is there any way of changing which icon is the default visible one on the toolbar?  For example, on Sketch (in Ordered), I use frequently use Rectangle by 2 Points, and rarely use Rectangle by Centre. Is there a way of switching it around so the one I use is visible on the toolbar, without having to go through the drop-down menu each time?

 

Many thanks in advance!

7 REPLIES 7

Re: Changing visible icons

Gears Phenom Gears Phenom
Gears Phenom

you have 2 options,

 

1.) customize the toolbar to show the tools you prefer

2.) set the option for last used on top.  this will keep the "by 2 points" on top of the pull-down for 1 click access.  This is not recalled between sessions however IIRC.  so you will need to select it 1x each session

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Changing visible icons

Pioneer
Pioneer

Thanks for the reply.

 

I've gone into the Customise Toolbar, and expanded to see the tool and drop down. I even managed to shift up the Rectangle by 2 Points so it is at the top, and saved it as a New Theme 1 (see attached).

 

However, I can't get it to become visible without expanding the drop down menu.  What do I need to do?

Re: Changing visible icons

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

I'd suggest customizing the ribbon to create the 'Rectangle by 2 Points' icon as a separate tool and ignore the pull-down.

Re: Changing visible icons

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

To elaborate on @Tushar's comment:

 

rect2points.png

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Changing visible icons

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Right. That's what I meant.

Thanks Bruce.

Re: Changing visible icons

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Tushar, Well I already did the work when I noticed your post. So I posted it anyway.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Changing visible icons

Pioneer
Pioneer

Thank you everyone for your help!