Cancel
Showing results for 
Search instead for 
Did you mean: 

Circles placed adjacent to protrusion edge.

Valued Contributor
Valued Contributor

I am stumped. Here is what I have got. I am new to this one and have some of the other assembly parts figured out, but this one is a little different. I have a cylinder, 3/4 inch tall, 1/4 dia, no reference planes, just protrusions, cannot edit them. There is a box, simple, let's say 8 inches by 8 inches. Now for the fun part. I have placed one side of the pin, flat side to the z-x plane.  Easy for that one.  Now, how do I place the same pin 2 inches from the bottom, and two inches from the left side protrusion. Do I need to use the in between measurement?  

 

Thank you. For your input. 

 

 

3 REPLIES 3
Highlighted

Betreff: Circles placed adjacent to protrusion edge.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Lex-luthor

 

 

just use a tangent relation from cylinder to plane.

 

For a tangent constraint You can use offset values as for most of the other relations.

 

Tangent with Offset and I hope I have read and understand Your request correctly.

 

See picture:

 

20170805_1741.PNG

regards
Wolfgang

Re: Circles placed adjacent to protrusion edge.

Valued Contributor
Valued Contributor
@hawcad

Awesome and thank you very much.

Kudos to you.

Re: Circles placed adjacent to protrusion edge.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Lex-luthor

 

 

 

Welcome and I'm happy to be able helping!

 

 

regards
Wolfgang