Cancel
Showing results for 
Search instead for 
Did you mean: 

Circular Pattern

Pioneer
Pioneer

If I want to add pattern 16 to pattern 18, Solid Edge crashes. Anyone an idea why?

4 REPLIES

Re: Circular Pattern

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If this was created in an Academic version, we will not be able to open the file.  Try posting to the "Solid Edge Student Edition Forum".



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com

Betreff: Circular Pattern

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Kurt,



 

I think the way You have treid to solve this design is not the best one for SE.

 

It is hard to see what You try to pattern where.

 

Get a smaller part with building a quarter of the part with all the feature in this segment a then  - finally - make a 4 time circular pattern of the body not of the features.

 

Also when patterning make fetaure groups before which You select for pattern afterwards.

And try to create a fast pattern rather then a smart pattern

 

 

Or and now I see that this here is a more or less irregular pattern not a 4 times circ.

 

Try to use the new Coordinate System Duplicate functionalltiy of ST9

Create a single "hole", group them to a feature group and cretae coordinate systems for refrence the other positions.

Then You can use the duplicate feature to get  the result 

 

 

 

regards
Wolfgang

Re: Circular Pattern

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

I suggest using Replace face command instead of extruding from face to face...

 

Here are steps:

 

BR, 

Imics
http://solidedgest.wordpress.com/

Re: Circular Pattern

Pioneer
Pioneer

Thanks, this has solved my problem