Cancel
Showing results for 
Search instead for 
Did you mean: 

Clip plane section colour

Builder
Builder

Section is shown as solid light blue colour when using the clip plane operation and the edge colours cannot be distinguised, how do I turn of solid fill on clip plane section or change the colour please ?

2 REPLIES 2

Re: Clip plane section colour

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In Options, View Settings, towards the bottom you will find the clipping plane settings.  If you set the plane colors to something and then set the Opacity setting down towards zero, the planes become transparent however the model will appear hollow.  The best way to get what you are wanting is to use PMI sections as they will maintain the part edge/face colors.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com
Highlighted

Re: Clip plane section colour

Builder
Builder

Hello Ken

 

Many thanks for the reply, the PMI section was exactly what I was looking for.

 

The clip plane command is for more quick viewing of sections.

 

Regards,

anthony