Cancel
Showing results for 
Search instead for 
Did you mean: 

Close Region

Creator
Creator

Hi,

 

I'm still new to Solid Edge! Smiley Happy

 

I am starting to draw the testdrive micrometer. I am drawing the first rectangle and it is supposed be drawn as a 'closed region'.

 

As i follow the instructions all i get is 4 seperate lines making up the rectangle.

 

Can anyone please tell me what settings i need to change so that when i create a shape it will automatically be closed when i finish.

 

Thank you,

Rob 

 

 

1 REPLY 1

Re: Close Region

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm not familiar with that exercize but to close up a multisided polygon use the trim corner command. That will trim and connect the ends.

Usually if you string the lines together they will be connected (unless you have "maintain relationships" turned off) so it's sometimes just the last line connecting to the first line that is missed.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200