Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Close spline without tangency continity

Pioneer
Pioneer

Hello all,

 

Is there a way to create a closed spline with no tangency continuity at the closure point ?

 

Thanks for your help

 

A.B.

2 REPLIES 2

Re: Close spline without tangency continity

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

The only way I know to do this is to start off the sketch with a 'point' object at the location of the closure point.  Then when drawing (or editing) the curve the two end points can be located exactly on the starting point.

 

SE recognizes the curve as closed (it can be extruded eg) although no tangent or curvature continuity is evident.

 

Hope that helps.

 

Frank

Edinburgh University

Re: Close spline without tangency continity

Pioneer
Pioneer
Frank,

Thank you very much.

Have a nice day.

A.B.