Cancel
Showing results for 
Search instead for 
Did you mean: 

Close this corner..sheet metal help

Is there a good way to close this corner?  I have messed with the contour flange options and cannot get it.  If I dont leave a gap, I get overlapping top flanges.  But leaving it open is not an option up top as it would be visible from the outside and manufacturing guy says thats a no-no.  I have attached file as well.  A short help video would be extremely helpful

 

Capture.PNG

1 REPLY

Betreff: Close this corner..sheet metal help

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @lifofadrafter

 

 

 

not shure what You want to get, but opening Your file shows me a fine contour flange corner if You add the vertical faces directly to that contour rather than making them extra as flanges

 

 

20180306_1722.PNG

 

regards
Wolfgang