Cancel
Showing results for 
Search instead for 
Did you mean: 

Cloud generating command for annotations etc... in SE Draft Environment?

Valued Contributor
Valued Contributor

Have I overlooked this or is there not a cloud generating command in the draft environment for SE?

 

If not are there plans for one?

 

 

4 REPLIES

Re: Cloud generating command for annotations etc... in SE Draft Environment?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
There is not one in the product. Not sure if there is one being planned. There was a macro somewhere that would would create them. Since it doesn't adhere to any of the drafting standards that I'm aware of, not sure many people actually care about it.


Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Cloud generating command for annotations etc... in SE Draft Environment?

Valued Contributor
Valued Contributor
Ken,

Thanks for the reply.

Although "The Cloud" may not adhere to any standards, it's a commonly used method to highlight important information in the approval process or in shop drawings where certain info needs to be highlighted visually to stand out..... depending of course on what industry the print hails from

Re: Cloud generating command for annotations etc... in SE Draft Environment?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
http://community.plm.automation.siemens.com/t5/Solid-Edge-Discussion-Forum/HOW-TO-CREATE-REVISION-CL...


Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

My quick & dirty solution is to draw a "cloud" with a ser...

PLM World Member Experimenter PLM World Member Experimenter
PLM World Member Experimenter

My quick & dirty solution is to draw a "cloud" with a series of arcs, then save it in the feature library.

To use it, just drag it onto the draft, where you can scale it or rotate it to suit.

You can save different sizes and shapes if you want to save time later.

I try not to use them unless I must

HTH

 

Alan