Cancel
Showing results for 
Search instead for 
Did you mean: 

Combining two dxf files

Experimenter
Experimenter
How do you combine two dxf files to make one drawing. I can copy the one dxf file into the other but I can't get it centered on the original drawing. Is there a tool to center it on the original drawing when bringing it in. Thanks for your help as I am a new user.
1 REPLY 1

Re: Combining two dxf files

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Boom,

 

If your two drawings are based on the same locale, relative to the origin, then it maybe just as simple as altering the option for "Preferred 2D Paste Behaior"......when in draft [blank, or existing] go to the Application button > Solid Edge Options > General tab, about midway down the selections.

 

ST8_DFT_SE-Options_General_2D-Paste.png

 

"Paste to selected position" will place it to match your cursor location......use that option, if you need to reorient the new geometry over the existing.

 

Maybe you could post some images, or even the files you want to merge.

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000