Cancel
Showing results for 
Search instead for 
Did you mean: 

Command Bar not visible for the Select command

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

In the Part, Sheet Metal, Assembly and Weldment environments, SE ST6, I am unable to see the Command Bar when the 'Select' command is active. For all other commands, the command bar appears. I am able to see the command bar for the Select command in the Draft environment however.

I have tried restarting Solid Edge and also the computer, also tried changing screen resolution, etc. to get the command bar back for the Select command. Is this behavior normal i.e. no command bar for the Select command except in the Draft environment?

1 REPLY

Yes, this is working as it should. The 3D environments do...

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, this is working as it should. The 3D environments do not have a command bar for the select tool. All options for the 3D select tool are set on the main ribbon.

 

Hope this helps,

Greg