Cancel
Showing results for 
Search instead for 
Did you mean: 

Commands Slow via Video

N/A

I Just had my computer checked... over the weekend checked out fine, I also checked my internet provider came out fine as well. I made a video to show how slow. The circle command took a little over 3 Min. to do 6 circles.

http://screencast.com/t/69Lw9sZCaj

Thanks
Crousie

8 REPLIES

Re: Commands Slow via Video

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi Crousie,
That sure doesn't look right....I placed a series of circles like what you have shown, in a matter of seconds.
To better understand what might be the cause of the issue....can you please list your computer specs?
Such as: CPU speed / RAM type / HDD type / Graphics type
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Commands Slow via Video

N/A
I hope is what you are looking for, I need to get the graphic type info. or will I need more Power!
http://screencast.com/t/eycHPq9M, http://screencast.com/t/AVxNEKrC31, http://screencast.com/t/onaCH2YK
Thanks
Crousie

Re: Commands Slow via Video

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi Crousie,
You might try a free application called SPECCY to gather system information like this.
http://www.piriform.com/speccy/download/standard

This is what I get....
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Commands Slow via Video

N/A
Hi Sean,
Here is a description of this computer. What is comparable from what I have to what you have, or any other Info you may have.
http://screencast.com/t/DNUfAZkT
Thanks
Crousie

Re: Commands Slow via Video

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi Crousie,
Well my first thought is that the onboard graphics is not really up to the task....but we are not talking about a very intensive task here.
Have you tried doing a complete shut-down and restart to clear any memory glutter that the system may be hanging onto?
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Commands Slow via Video

N/A
Hi Sean,
Shut down didn't do the trick. So, what brand of and possible specks for a graphics card for Solid Edge and or would I have to upgrade from W7 Home Premium?
Thanks
Crousie

Re: Commands Slow via Video

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi Crousie,
Well given that you're using a laptop, upgrades of this nature are basically impossible....seing as it's not simply a replacement of existing hardware, as it isn't there.
Although it certainly shouldn't have stopped you in this case.....but computers with "dedicated" graphics is almost a must for all resource demanding applications, the likes of Solid Edge. There is a definite trend, based on driver stability, towards using nVidia based cards, but ATI units work well also...just requires matching it to the right driver, which can sometimes be an older one.
Am at a bit of a loss as to the actual root cause of your issue....hopefully someone from developement is lurking with a clue to nailing this for you.
Regards,
Sean Cresswell
Streetscape Limited (NZ)
-
Sent from my Samsung Galaxy NoteII using Tapatalk 2.
-
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Commands Slow via Video

N/A
Hi Sean,
Thank you for your knowledge and support with this issue.
Thanks
Crousie