Cancel
Showing results for 
Search instead for 
Did you mean: 

Computers Freezing

Experimenter
Experimenter

I am using the latest edition of Solid Edge 10 in my classroom. My students are just starting Class 2. Today, when they came into class, I had them open up a Metric Part file to begin designing in 3D and all but 1 of the programs froze. Only one student was able to draw 3D shapes and all the others froze, even after restarting the computer and re-opening Solid Edge. 

 

Any ideas on how to fix this?

 

I didn't have this problem during class 1 when students were drawing 2D shapes in Metric Draft. 

1 REPLY

Re: Computers Freezing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @MrJulian,

 

That is unfortunate to hear......however, it is difficult to offer a possible solution, without some supporting information, such as what operating system [especially if  running Windows 10, with Fall Creators Update] as there are counter measures on offer there, as are system drivers, and normally graphics card drivers is the area to look at.

 

Can you provide some more indepth detail around these areas please?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000