Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Configurations: use a custom one when insert an assembly into another.

Pioneer
Pioneer

Hi!

I dont't konw if is possible insert an assembly into an assembly (father) directly with a custom configuration.

It is useful for me when I must instert a big assembly into another.

When I insert it, I must wait the loading. I think that I could make before a configuration in the assembly (child) with only visible the parts that I use for positioning it, and save time.

Is possible?

 

Thanks

2 REPLIES 2

Re: Configurations: use a custom one when insert an assembly into another.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yes it is.  Before inserting it, right mouse click in the Part Library pane and select "Assembly - Use Configurations and Open As Settings".  Then when you add an assembly as a component you will be prompted with a dialog and can select the Configuration to use for placement.

2017-05-16_17-09-58.png



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Configurations: use a custom one when insert an assembly into another.

Pioneer
Pioneer
Thank you!