Cancel
Showing results for 
Search instead for 
Did you mean: 

Connect Mate

Valued Contributor
Valued Contributor

ST7 Q:

 

When and why did the Connect mate change so that you cannot pick faces anymore? 

Example: Mating the cones on a hydraulic adaptor; we were able to connect these two faces together.

 

Thanks


G

3 REPLIES

Re: Connect Mate

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm not following or having any difficulty with connects. I'm on ST8 now but don't recall issues with ST7. You can only pick one face though. The other component has to be a keypoint, an edge, or axis.

Maybe a screenshot would help understand what's happening for you.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Connect Mate

Valued Contributor
Valued Contributor

All of our hydraulic adaptors have the mates saved so when placed the connect is from the taper face on the adaptor and we used to be able to (in ST6) select the taper on the part to be mated to. Now we are presented with every option accept the tapered face.

 

 

Re: Connect Mate

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I've never known connect to work between two faces.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200