Cancel
Showing results for 
Search instead for 
Did you mean: 

Connecting Splines

Experimenter
Experimenter

Hello,

 

I have recently made an airfoil using splines, and tangent curves. I have turned the tangent curves into splines, and now I would like to turn all connected splines into a single entity/spline.

Does anyone know if that is possible?

I am trying to judge the curvature using the curvature comb and need the whole outline to be a single spline in order to be able to read the curvature properly.

 

Many Thanks,

 

Boris

5 REPLIES

Re: Connecting Splines

Phenom
Phenom

Hi @Dominis

 

did you try to use Curve - Close Curve function ?

 

Untitled.png

Re: Connecting Splines

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Based on your description, the 'Derived Curve' command appears to be best suited for the purpose.

 

DerivedCurve01.png

 

~Tushar

 

Re: Connecting Splines

Experimenter
Experimenter

The close curve option won't work, I'm not trying to close a curve, i'm trying to join existing curves together.

 

As far as the Derived curves goes, It will not let me turn the outcome entity into a spline, so I am not able to make a curvature comb to examine the curvature.

 

Thanks for trying though guys!

 

Re: Connecting Splines

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hello @Dominis,

 

No, there is currently no such functionality in Solid Edge to do what you seek.....you can of course use relationships to connect & make tangent, etc,....but nothing that "converts" multiple entities [Lines, Arcs, Curves] into a "single" entity.

 

In my mind, your only course of action, would be to [assuming you're in a s"ketch" of a 3D model]  create a new sketch, and trace over your other geometry to make a new "single" curve to capture all you need.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Connecting Splines

Experimenter
Experimenter

Ok, thanks very much Sean, I appreciate the help!

 

Boris