Cancel
Showing results for 
Search instead for 
Did you mean: 

Constraining distance between planes into assembly

Pioneer
Pioneer

Coming from a Creo background, I'm used to creating parallel constrains, dragging my part where I want it, then changing the parallel constraints to distance constraints.  Alternatively, I could fix (ground) my part, then add my distance constrains, then delete the fix/ground constraints.

 

In solid edge ST8, is there a way for me to take my grounded component and directly apply a distance constraint (so I can then remove my grounded constraints) or is it necessary that I record measurements, delete ground, mate surfaces, and then apply the distance?

5 REPLIES 5

Betreff: Constraining distance between planes into assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

You simply can change the x,y z position of grounded parts with properties of occurence.

RMB at pathfinder

 

 

 

regards
Wolfgang

Re: Constraining distance between planes into assembly

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Hi Patrick,

 

I believe what you want to do is use the mate constraint, but select the float option when placing the constraint.  You will see the distance entered in the box, but not yet applied.  Then go back and change the float option to fixed and SE will apply that value and your part should not move.

 

The same idea works for planar constraint as well.  

 

You'll need to suppress or delete the ground constraint before doing the above steps.

 

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1
Highlighted

Re: Constraining distance between planes into assembly

Pioneer
Pioneer

That's what I was missing, thank you!

Re: Constraining distance between planes into assembly

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Glad to help!

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: Constraining distance between planes into assembly

Phenom
Phenom

You can also try using the 'Use Distance Between Faces as Default Offset' setting.

If your part is positioned and you delete the ground constraint it should stay in the same place.

I should point out that it does not work with flash fit.

You have to specify whether Mate or Align.

The setting stays on until you turn it off again.

 

Maintain Offset.JPG

 

 

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.