Cancel
Showing results for 
Search instead for 
Did you mean: 

Constraints question

Phenom
Phenom

Hi,

 

I am facing the problem with displaying the constrained lines.

On the sketch I can see that some of the line are under constraint - but they are.

On the 3D Part  environment I can see that this part is constraned.

 

Can you please tell me where is the issue ?

 

thank you,

 

Arek123.png123b.png


Production: SE ST10 MP8
;
6 REPLIES

Re: Constraints question

Gears Phenom Gears Phenom
Gears Phenom

you are missing some tangent relationships in the corners and also some of the wall thickness values are not driving dims.

 

Might i suggest however that for this model that you only sketch the outside profile and then use the 3D command  THIN WALL. 

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Constraints question

Legend
Legend
Might even consider doing a square shaped protrusion, radius the edges, and then thin wall. No real need to do a sketch, for this instance, IMHO.

Re: Constraints question

Phenom
Phenom

Hi @Johnson_BigMatt,

 

thank you for your reply,

 

Well, after restarting the computer this sketch became constrained itself.

 

So, strange behaviour.

 

Regards,

 

Arek


Production: SE ST10 MP8
;

Re: Constraints question

Phenom
Phenom

Hi @Trikefreak

 

Thank you for your reply,

 

Yes, this is a next method to build this part. You can do it on many different method.

 

regards,

 

Arek


Production: SE ST10 MP8
;

Re: Constraints question

Legend
Legend

@Trikefreak,

I think frame generator needs cross section sketches like this, as it just does a protrusion of the selected cross section, but not sure.


Those who know me question the assigned user rank.

Re: Constraints question

Legend
Legend
Always best to be sure!