Cancel
Showing results for 
Search instead for 
Did you mean: 

Continuously increasing radius in circular segment

Experimenter
Experimenter

Hi together,

 

I have to draw a circular segment where I have a start and end radius. Is there a way that the radius between both fix points will increase constantly over the entire route?

 

Regards

2 REPLIES 2
Highlighted

Re: Continuously increasing radius in circular segment

Gears Phenom Gears Phenom
Gears Phenom

The Spiral Type of Helical Curve should help you out here.

Helical Curve Spiral.jpg


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Continuously increasing radius in circular segment

Experimenter
Experimenter

Thank you Matt,

that worked very well.