Convert to Sheetmetal...

Valued Contributor
Valued Contributor

Hi~

You want to convert from part to sheet metal using the feature in the title.
Using this function, it is not possible to show the shape of cut as shown in "Figure 3".
What should I do?

11.png22.png33.png

8 REPLIES

Re: Convert to Sheetmetal...

Esteemed Contributor
Esteemed Contributor

Hi there @Hclee,

 

Draw sketch lines at those corners, and use the "Rip" step on the "Thin Part to Sheet Metal" ribbon bar, to include the sketches and natural corners.....and you're done. Rather than the "Part To Sheet Metal" command, in these more complex transformations.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Convert to Sheetmetal...

Valued Contributor
Valued Contributor

Thankyou for Answer..

 

Yes ...
I can not ...

Re: Convert to Sheetmetal...

Honored Contributor
Honored Contributor

Hi 

 

 

the RIP step also can be done directly from point to point without the need for an extra skecth.

This is important if You have many of those situations to be solved.

 

 

Just hit the "R" key and click point to point for creating those split lines

 



regards
Wolfgang

Re: Convert to Sheetmetal...

Valued Contributor
Valued Contributor

HI hawcad

I am very curious about the "R" keyboard you mentioned. Does this apply to corner ripping?
This is the first time I hear it.
Do you have any pictures or videos ...?
I wonder how it is used.

Re: Convert to Sheetmetal...

Honored Contributor
Honored Contributor

Hi @Hclee

 

 

what does Your Command Bar say during the converting process?

Is there any information about the "R" key?

 

 



regards
Wolfgang

Re: Convert to Sheetmetal...

Honored Contributor
Honored Contributor

Hi @Hclee

 

 

just started an English Solid Edge version to see what the Command Bar will show at this moment and this is what I see here:

 

20170719_2030.PNG

 

 

And here is what the result look like:

 

20170719_2035.PNG



regards
Wolfgang

Re: Convert to Sheetmetal...

Valued Contributor
Valued Contributor

Thank you very much.
The prompt bar could not be checked because it was hidden in the beginning.
You are the best .. ^^

Re: Convert to Sheetmetal...

Honored Contributor
Honored Contributor

Hi @Hclee

 

 

 

that's as I always say:

"Take care about to have the Command Bar well situated on Your screen (I like it a little bit bigger below the pathfinder) then increase the text size so that everything could be read at anay time."

 



regards
Wolfgang