Cancel
Showing results for 
Search instead for 
Did you mean: 

Convert to Solid body

Valued Contributor
Valued Contributor

Hi Edge users ..
I downloaded the STEP file and opened it.
Opened as a surface body.
I want to make this solid.
Using all the methods I know, this shape could not be converted to a solid.
I am looking for a way to easily convert.
Help me ^^

 

Version : ST9

 

Is there a way to easily identify the wrong part?
I would appreciate if you can let me know where you can convert to solid.

8 REPLIES 8

Betreff: Convert to Solid body

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

if You run the "Show Open Surfaces" command this shows You the big hole in Your surface body.

 

Repair it and YOu will succedd.

 

20170523_1105.PNG

regards
Wolfgang

Re: Convert to Solid body

Experimenter
Experimenter

Hello,

 

you first have to look where to stitch the surface.

Here you have to first delete a plain then create a surface and stitch.

 

Wolfgang

Betreff: Convert to Solid body

Valued Contributor
Valued Contributor

Hi hawcad
I am always thankful for your reply.

But this part is not easy to repair.
I want to know how to repair it.

Betreff: Convert to Solid body

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi:

 

I have attached a short video here:

 

 

Hope this helps.

 

 

Betreff: Convert to Solid body

Valued Contributor
Valued Contributor

Hi Tushar And wziegle
I watched the video well ..
I tried similar but it did not work.
This method seems to consistently vary depending on how the surface body is opened.

This way, I would like to have to touch each other with craftsmanship.
Thank you for answer.

Betreff: Convert to Solid body

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Tushar

 

 

 

thanks for answering so fast.

This exactly is what I also did.

 

Optimize, Search for "Non-Closed-Surfaces", Delete/Repair, Stitch, Convert

 

Good Job!

 

regards
Wolfgang

Betreff: Convert to Solid body

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

there always should be Your first step to run the "Optimize Geometry" when opening an imported part.

 

This saves a lot!

 

 

Very surprising here is, that the geometric problem only occurs on one side while the other (symmetric) is OK)

Here the better question also is: "Wherefrom is this geoemtry coming?"

Which software are they using and can You get a different file format?

 

Maybe the export of the geometry went wrong, so taht any import will automatically be unable to do it successfull

 

regards
Wolfgang

Betreff: Convert to Solid body

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@Hclee wrote:


I tried similar but it did not work.


That is very unfortunate.

This is a much standard procedure for bad surface bodies.

Thanks Wolfgang @hawcad for confirming that you'd follow the same process and that you were able to repair the part. Else it would have been so much bandwidth gone waste.