Cancel
Showing results for 
Search instead for 
Did you mean: 

Coordinate Dimension Jog After Placing

N/A
I'm having problems adding a jog in a coordinate dimension after placing the dimension. I can add the jog while placing the dimension but not after placing it. The help files says "You can also use the Select Tool to add or remove a jog on an existing coordinate dimension by holding the Alt key." but that doesn't work for me. Is this a bug in the program or an error in the help file?

Thanks.
3 REPLIES
Highlighted

Re: Coordinate Dimension Jog After Placing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
The process is:
Select the Dimension line
While holding the ALT key, select point where you want the jog (two handle points created)
Release the ALT key
Drag 2nd handle point to desired jog location


Ken

Production: ST10 MP6
Testing: SE 2019

Re: Coordinate Dimension Jog After Placing

N/A
Thank you. It works for me now. I think I was holding down the ALT key when I first selected the dimension line and that was what was screwing me up.

Re: Coordinate Dimension Jog After Placing

Experimenter
Experimenter

In Solid Edge ST8 the correct command sequence is 

1) hold the ALT key

2) double click the dimension witness line

Then you can move the jog or dimension text to the position you desire.