Cancel
Showing results for 
Search instead for 
Did you mean: 

Coordinates 2D photo

Pioneer
Pioneer

Is there any way to get the coordinates to a 2D photo and create a 3D object ? For example, take a picture a few legs, then I can take the measures and the actual shape of the legs? 

 

Best Regards,

Jorge Ferreira

18 REPLIES 18

Re: Coordinates 2D photo

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Pakito,

 

This post seems in direct relation to your other "Leg 3D" one.

 

To answer it,.....yes you can, but you'd need to have a scale item on the photo, and then you'd also need enough [side view perhaps] information to make any 2D information gathered, into 3D. [IE: curvature, depth, etc]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Coordinates 2D photo

Pioneer
Pioneer

More specifically what he needed?

Re: Coordinates 2D photo

Siemens Phenom Siemens Phenom
Siemens Phenom

There is third party software available that will allow you to digitize and build 3D CAD models from 2D photos.  However, these tools typically require multiple photos taken at different angles with common hard points to select between the photos.  IMHO, unfortunately a human leg does not make a good subject for 2D photo digitizing because there are no real hard points to pick on.

Highlighted

Re: Coordinates 2D photo

Pioneer
Pioneer

So it's hard to create a 3D leg through a 2D photo? What kind of angles should have the pictures and what procedures?

Re: Coordinates 2D photo

Siemens Phenom Siemens Phenom
Siemens Phenom

First you will need to find and install some third party software that will allow you to create the digitization from photos.  Then follow whatever procedures *that* software requires in order to complete the digitizing. 

 

Typically the more pictures you have that are taken from multiple angles with multiple common hard points to tie the shapes together the more accurate the result.

 

However, as previously stated such solutions require hard points that are common between the photos to be of any success.  What hard points do you think there are on a shin/leg?

 

IMHO, for something as free flowing as a human leg you would be better served with a  3D scan.

Re: Coordinates 2D photo

Pioneer
Pioneer

What is referred to as hard points? Hardness type stone, wood, plastic, etc? Cinnamon in a tight spot would be in this case the tibia and fibula together. What software can I use to do the job of creating 3D through 2D?

The 3D scanner always implies being in contact with the person, but I also wanted to make a mold at bay.

Re: Coordinates 2D photo

Siemens Phenom Siemens Phenom
Siemens Phenom

If you were to take photos of soemthing as simple as a box you have multiple hard points that show up in the photos that you can then digitize against-- the corners of the box make hard points.


There are  no naturally occurring corners (hard points) on a leg.  You would have to place markers on the person's leg to ensure that you then have common points between the photos taken so that you can digitize the shape.

Re: Coordinates 2D photo

Pioneer
Pioneer

Imagine you ask me to send you pictures to make the mold. What kind of photo you could send and where you had to point out the points?

Re: Coordinates 2D photo

Siemens Phenom Siemens Phenom
Siemens Phenom

@Pakito I suggest you go find some application to scan 2D photos into 3D models, download it, install it, and just give it a try.  That way you will then get a better understanding on how such software works and what you would need to accomplish your end goal.